If you implement any of the edits below, the model will be recognized as "Not standard parts."
When a different dimension value is entered after read-only dimensions are removed
When features are added
When a model is added, deleted or replaced
When a configuration is added
If you need to add a feature or configuration, only do so after saving the part number with "Reduce file size" enabled.
        See here for detailed instructions.